Part Number: EZ430-T2012
I need the connector part number for this board please .. i use the ez430 as a programmer tool and need to have the same mating connector as on the EZ430-T2012 part
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
It's a standard 1.27 mm (0.05 ") header with machined pins. Anyway, the EZ430-F2013 User's Guide says:
9 Frequently Asked Questions
6. What are the part numbers for the connectors between the MSP-EZ430U emulator and the MSP-EZ430D target board?
Header: Mill-Max 850-10-004-20-001000 (Digi-Key part number ED8650-ND)
Socket: Mill-Max 851-93-004-20-001000 (Digi-Key part number ED8850-ND)
**Attention** This is a public forum