Other Parts Discussed in Thread: AMC1204, , MSP430F6779A
Hello,
the max. frequency stated in the datasheet is 2.3MHz. But it is mentioned as "Modulator...". So, if I'll only use the decimation filter for an external applied bit stream via the portpins: What max. frequency I'm allowed to apply to the SD24 module, the same?
If it is allowed to use a higher frequency (e.g. 5MHz) and I want to use also a sigma-delta-modulator: I think I'll have to switch the frequency, before using the analog part.
Thanks in advance!