Other Parts Discussed in Thread: MSP430F5529,
Hi,
We are bringing up boards with MSP430F5659 devices which are an alternate for us from the MSP430F5529 devices, and apart from the different device, the crystals, capacitors, etc are identical between the boards.
We can't get the XT1 LF 32.768K oscillator to start on MSP430F5659 despite trying everything from different crystal manufacturers to different capacitor values. The crystal setup and clock setup code work perfectly on MSP403F5529.
There is no errata, no port pins that need configuring and nothing else that we can see that could cause the XT1 not to start.
Would anyone know if there are any specific differences between '5529 and '5659 variants with respect to the TX1?
Thanks
Stomp!