Hi,
I have a voltage regulator that will likely have a few 100mV of voltage ripple that will be feeding the MSP430G2755. Is there any concern on normally operation of the MSP430 with this much ripple?
Regards,
Jake
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have a voltage regulator that will likely have a few 100mV of voltage ripple that will be feeding the MSP430G2755. Is there any concern on normally operation of the MSP430 with this much ripple?
Regards,
Jake
It is normal practice to eliminate such ripple with LC, RC filter or using LDO or/and adding additional capacity decoupling buffer. What can affect with this ripple? Probably any analog functionality including ADC, DAC, Capacitive Sensing, buttons/switchers debouncing filters, comparators and so on...
Regards,
Alexey
Jacob,
Every MSP430 MCU has internal LDO for Core logic (usually it is an internal 1.2V low-side bus) . So, CPU, memory and so on is protected from such ripple by default. But high-side bus peripherals are not. The latest generation of MSP devices like FR59XX has quite fast peripheral gate logic time lag for semiconductor elements, but for older models like FR69XX or even FR41XX it has 4 times longer switching time. In such transitions the ripple can 'hit' many times gate threshold voltage or can significantly decrease noise immunity for external digital communications. That is, every 'digital' signal differs from pure sine-wave only by spectrum, the first one has fundamental sine wave frequency and its infinite (in theory, practically limited by inductance, resistance and capacitance of trace paths) number of sine-wave harmonics, but in the second one has only one sine wave, theoretically goes in spectrum to only fundamental frequency.
Regards,
Alexey
PS: but since the MSP430 is actually low power device, it is easy to filter 120Hz ripple with RC low-pass filter with 50 Ohm resistor with 100 uF low-voltage capacitor. Current flow will be limited in MCU to 20mA, but this is also a good practice to protect MCU from malfunction in such cases as reverse polarity.
**Attention** This is a public forum