Running the application directly out of the box works fine. After reprogram the board with the provided binary, application works fine. When I build using IAR EWW 6.30.1 application resets when I try to invoke the FRAM logging, whether I am debugging or running stand-alone.
When I debug, if I set a break point on line 140 of main.c (dataArray[12288] = 0;) and then try to single step the board will reset.
If I change the breakpoint to line 139 of main.c (storeTimeStamp();), I can step into the function call and then board resets on the first statement of that method.
Any suggestions as to what is wrong? I did have to update the workspace and project files when I started trying to work with the source.
Jim