Hi together,
I bought recently an used MSP-FET430UIF from eBay and it seems it is faulty.
In Device Manager it appears as "MSP430 Application UART" but I get "MSP430.dll Initialization error". I tried on different 3 PCs (Windows XP, 7) with different versions of CCS, tried with Elprotronic Lite software and nothing. If it is seen by windows as "MSP430" device I guess the EEPROM contect is not altered so the MSP430F1612 could have a stuck firmware. I don't have another JTAG programmer to flash it. How can I flash it ? Is the BSL not deactivated on it ? I have 2 Launchpads if could help.
What I wanted to do with this FET is just to blow fuses. I was thinking about using the hardware part from "FET" in combination with LP in order to blow fuses over SBW.
Many thanks