Hi,
When MSP 430 is running on battery, rarely RTC value is read with strange value.
It is highly likely that the RTC year has reached 2099 or more from the value after occurrence.
It occurs when only RTC and WDT are operating.
(The probability of occurrence of this problem is quite low.)
Checking that READY is set in the program, RTC reading is done.
Even on the board where the problem occurred, the batteries were not running out,
RTC time merely goes wrong, there are no problems with other operations.
Q1:
Is not there any cause or countermeasure that might cause such a problem?
Q2:
Does such a problem occur when the supply voltage drops?
Regards,
Da