I have a question about pins of MSP430F47176.
According to pdf file (msp430f47176.pdf) page 10, there are two pins which used as "TDI".
That is, PIN96 (TDO/TDI) and PIN97 (TDI/TCLK).
The pdf shows that
TDO/TDI (pin 96) -- Test data output port. TDO/TDI data output or programming data input terminal.
TDI/TCLK (pin 97) -- Test data input or test clock input. The device protection fuse is connected to TDI/TCLK.
Is the TDI of pin 96 used only for program downloading from PC to MSP? Or are there any other occasion where
data is transferred from MSP to PC, such as during debug mode?