Hi Team
GPN: MSP430F5234
Hi
Please can you tell me what is the maximum input leakage or bias current for the Comparator_B input pins of an MSP430f5234.
All page & section numbers mentioned below refer to the following datasheet;-
http://www.ti.com/lit/ds/slas897a/slas897a.pdf
Section 5.40 on page 44 shows that the Comparator_B common mode input range is 0 to Vcc-1 volts.
Section 5.9 on page 23 shows that the high-impedance leakage current is a maximum of /-50nA with Vss or Vcc applied to the pin.
However I cannot find any mention of what the maximum comparator input pin leakage current is when the applied voltage is at intermediate values between 0V & Vcc-1V.