I have code that was getting optimized out because I believe there is a macro definition issue in the MSP432 SimpleLink DriverLib.
I'm using : simplelink_msp432p4_sdk_2_10_00_14
I get the interrupt flags from SPI_getEnabledInterruptStatus
//***************************************************************************** // //! Gets the current SPI interrupt status masked with the enabled interrupts. //! This function is useful to call in ISRs to get a list of pending //! interrupts that are actually enabled and could have caused //! the ISR. //! //! \param moduleInstance is the instance of the eUSCI A/B module. Valid //! parameters vary from part to part, but can include: //! - \b EUSCI_A0_BASE //! - \b EUSCI_A1_BASE //! - \b EUSCI_A2_BASE //! - \b EUSCI_A3_BASE //! - \b EUSCI_B0_BASE //! - \b EUSCI_B1_BASE //! - \b EUSCI_B2_BASE //! - \b EUSCI_B3_BASE //! //! Modified registers are \b UCAxIFG. //! //! \return The current interrupt status as the mask of the set flags //! Mask parameter can be either any of the following selection: //! - \b EUSCI_SPI_RECEIVE_INTERRUPT -Receive interrupt //! - \b EUSCI_SPI_TRANSMIT_INTERRUPT - Transmit interrupt // //***************************************************************************** extern uint_fast8_t SPI_getEnabledInterruptStatus(uint32_t moduleInstance);
Note in the comment refers to (EUSCI_SPI_RECEIVE_INTERRUPT and EUSCI_SPI_TRANSMIT_INTERRUPT).
These mask macros are also used by:
- SPI_getInterruptStatus
- SPI_disableInterrupt
- SPI_enableInterrupt
When i look at how the macros are defined you get the following in (ti/simplelink_msp432p4_sdk_2_10_00_14/source/ti/devices/msp432p4xx/driverlib/spi.h)
#define EUSCI_SPI_TRANSMIT_INTERRUPT EUSCI_B_IE_TXIE_OFS #define EUSCI_SPI_RECEIVE_INTERRUPT EUSCI_B_IE_RXIE_OFS
Now the concern is EUSCI_B_IE_TXIE_OFS and EUSCI_B_IE_RXIE_OFS refer to bitmap offsets rather than the bitmap value. This can be seen in: (ti/simplelink_msp432p4_sdk_2_10_00_14/source/ti/devices/msp432p4xx/inc)
/* EUSCI_B_IE[RXIE] Bits */ #define EUSCI_B_IE_RXIE_OFS ( 0) /*!< UCRXIE Bit Offset */ #define EUSCI_B_IE_RXIE ((uint16_t)0x0001) /*!< Receive interrupt enable */ /* EUSCI_B_IE[TXIE] Bits */ #define EUSCI_B_IE_TXIE_OFS ( 1) /*!< UCTXIE Bit Offset */ #define EUSCI_B_IE_TXIE ((uint16_t)0x0002) /*!< Transmit interrupt enable */
Note that EUSCI_B_IE_RXIE_OFS which defines EUSCI_SPI_RECEIVE_INTERRUPT is 0, so any mask checks against it, will always fail. So the code below was always getting optimized out.
if( flags & EUSCI_SPI_RECEIVE_INTERRUPT ) { /* USCI_B0 TX buffer ready? */ while (!(SPI_getInterruptStatus(pCtxt->module, EUSCI_B_SPI_TRANSMIT_INTERRUPT))); rxData = SPI_receiveData(pCtxt->module);
I can correct this using my own definition for the interrupt mask bits.
However I would like to know if am I misunderstanding the comments about the "mask" macros, or is there a bug in the macro definition?
Or the other possibility did I accidentally copy/paste over the macro when digging into the header files for the macros?