I want to run the MSP430G2231 at 8 or 16 MHz. According to the datasheet, the device has internal calibration information to achieve this speed.
When I look at the MSP430G2231.h file, I find DCO and BCS calibration pointers to the 1MHz speed, but no other clock speed.
On the io430G2231.h file, however, the pointers to the internal address containing the 16 MHz calibration are provided.
Is this an oversight on the MSP430G2231.h file, or should I assume that the data on the 0x10F8 (for DCO) and 0x10F9 (for BCS) is not to be trusted?
I found another post on this forum stating there are some tools from ElProtonic to do the 8 or 16 MHz calibration. Can I get a link to the exact tools that would allow me to find this info?
Is there any other way to easily achieve the 8 or 16 MHz frequency with good precision?
Thanks for your input! Best regards,
JIQ