1.The customer feedback our LSA1420 table fixed value to appear the confusion phenomenon,Use the simulator to view the fixed value parameters as shown in the figure below:
The starting address of the value parameter :0x025a00
The fixed value parameter is shown below:
2.As described above, the internal Memory storage of MSP430F5418 is abnormal,But some of the Numbers are strange, like "37" and "05".How do these variables come about?
Does the above abnormal situation occur when Memory is frequently erased in a short period of time?MSP430F5418 internal FLASH wipe life is what?
This table has been installed on the site for only more than 2 months now, is it caused by the above problems caused by too many times of wipe or storage exceptions caused by other reasons?