Part Number: MSP432P4011
Hi MSP Team,
One of my customer is attempting to program flash of MSP432 using MSP-FET + MSP-FET-432ADPTR at 1.8 V. However, the programming fails repeatably when supply voltage at MSP432 is 1.794 V, but is successful repeatably when supply voltage at MSP432 is 1.803 V. Target Voltage setting in CCS is 1800 mV for both these tests. This is also repeatable using the MSP432P4111 eval board. We are able to connect to MSP432 in either case and adjust register values, but not able to write to Flash at the lower voltage setting.
I understand the 1.794 V is above the recommended operating conditions. Have you seen this issue before? Any insight on what may be going on?
Thanks
Leo