Dear Sir,
I have asked some question about the tidud25a before,
recently, i need to go implement more test on it ,
my test board was CC1310 Launchpad and custom LC board (mainly refer to the given schematic)
for the pdf , i refer to
for the schematics ,
i refer to the one used in
i have encounter some new problem and would like to ask .
here is my question:
1) I have test the two inductors case, i find the waveform is a bit strange as follow:
this is one of the waveform i captured from the point of the receiver leg of CC1310,
which i think is ok or good.
However, some other waveform appears is not good?(but it still return the tick value)
and for the second question:
2) For the sampling rate , in P.6 Section 2.3.3 it mentions about it, and i have changed the value(RTC ?) from default 16 to above,
so is the RTC value in CCS equal to the sampling rate ?
And when i increase the value, the overall EFF count give more error, how can i solve it?
3) in the scs, it have a variable call LUT , and it is 16(default),
the desciption of it is Length of Tables for counters (Up,down, error), can you explain more what is it?
thanks
Jeff