Part Number: MSP432P401R
What's the difference between PM_TA0.1 pin and lead TA2.4 without PM name using the capture mode function of request interrupt?The same configuration method TA2.4 can be used frequently, and PM_TA0.1 can not be used.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP432P401R
What's the difference between PM_TA0.1 pin and lead TA2.4 without PM name using the capture mode function of request interrupt?The same configuration method TA2.4 can be used frequently, and PM_TA0.1 can not be used.
PM_TA0.1 selects timer_A0, why there is a PM name in front of it, plus the PM name in the Port Mapper class, most of it does not add in the Timer class, whether the use of capture mode is different between the two classes, I configure the same mode, capture the waveform with capture mode, the same waveform timer_A2 and timer_A3 capture the waveform to get The interrupt counter value is correct, the interrupt counter value obtained by timer_A0 is relatively large, and the value obtained is constantly changing.
**Attention** This is a public forum