Hi again,
I've asked a couple of questions previously, and we're continuing to work with the EMDC library (on an MSP430F67621A, with some changes made to the ADC parts of EMDC to support the ADC10 unit in this part).
We're now looking at calibration, and the measurements that are available from the library.
One thing we've noticed is that there is not a "phase angle" value available to read back - there is only the "power factor". Initially we thought this would be fine (of course the two are inherently related), but after looking more closely at the results obtained after calibration, in particular by changing the "active power scaling factor" and the "reactive power scaling factor", it seems like the power factor is calculated from the magnitude of the active and reactive power. Mathematically this is fine, that is what the power factor is a measurement of, but the problem we have is what to do with the two different power scaling numbers - changing one of the factors but not the other will cause a change in the reported power factor.
I have the following questions:
- How come there is no actual "phase angle" value available from the EMDC library?
- What is the intention behind the separate active and reactive power scaling numbers?
- Wouldn't the power factor come directly from the measured phase angle between the voltage and current waveforms?
- Why does power factor instead seem to be calculated from the scaled active and reactive power? (which themselves presumably must be calculated from the phase angle)
This makes it hard for me to comprehend how calibration is meant to work - it is possible to change both the integer shift and preload values in the "phase correction" setting to adjust the power factor, as well as changing the separate active and reactive power scaling factors. Essentially, there are more inputs than outputs to solve for, what is the recommended approach for calibration? For example, suppose we apply a known test load with a power factor of 0.5, and then adjust the phase correction to have this be reported correctly (or as close as possible). Why would we not use the same scaling for active and reactive power? Surely using these to achieve a correct power factor at 0.5 would just make the measurement incorrect at other power factors?
Thanks for your help.