Other Parts Discussed in Thread: ENERGIA, , MSP430FR5739
Hi,
I just bought a MSP-EXP430FR5739 experimenter board. The idea is to program it using the Energia GUI, which is what I've been using at the university. So I installed the drivers for Winx64-bit (Windows 10) and downloaded Energia 1.8.7E20. I wanted to do a quick test to make sure that I could communicate with the board, so I tried uploading one of the basic examples, Blink.ino. From the tools menu, I selected the board type and the COM port that was assigned by my laptop, COM4. But when I clicked the upload button I received this message:
Sketch uses 972 bytes (6%) of program storage space. Maximum is 15743 bytes.
Global variables use 20 bytes (1%) of dynamic memory, leaving 1004 bytes for local variables. Maximum is 1024 bytes.
MSPDebug version 0.24 - debugging tool for MSP430 MCUs
Copyright (C) 2009-2016 Daniel Beer <dlbeer@gmail.com>
This is free software; see the source for copying conditions. There is NO
warranty; not even for MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.
----------------- NOTE ------------------
Modified version of mspdebug for Energia
Do not use standalone
-----------------------------------------
Chip info database from MSP430.dll v3.3.1.4 Copyright (C) 2013 TI, Inc.
Using new (SLAC460L+) API
MSP430_GetNumberOfUsbIfs
MSP430_GetNameOfUsbIf
Found FET: HID0010:COM4
MSP430_Initialize: HID0010:COM4
Firmware version is 20409001
MSP430_VCC: 3000 mV
MSP430_OpenDevice
MSP430_GetFoundDevice
Device: MSP430FR5739 (id = 0x00ab)
3 breakpoints available
MSP430_EEM_Init
Chip ID data:
ver_id: 8103
ver_sub_id: 0000
revision: 24
fab: 55
self: 5555
config: 24
Device: MSP430FR5739 [FRAM]
MSP430_Run
prog: 'C:\Users\User1\AppData\Local\Temp\arduino_build_834523/Blink.ino.hex': The filename, directory name, or volume label syntax is incorrect.
MSP430_Close
An error occurred while uploading the sketch
As far as I can see, the software (Energia) is detecting the MSP board on COM4 and there is communication with it (the board reported some firmware and hardware data back to Energia), but apparently the file 'Blink.ino.hex' could not be found or read by Energia to load it up on to the board. I checked the path to this file and it is correct, the file is there and I could open it and see Hex data inside (as you would expect).
Any ideas of what could be happening?
Cheers.