Other Parts Discussed in Thread: MSP-FET, ENERGYTRACE, UNIFLASH
Hi!
I have been measuring the power consumption with the MSP-FET and also using a battery and a multimeter on the I_meas jumper. I have set the settings to the same as in this guide and disabled LCD, Buttons and removed jumpers J1,2,3,5 and I have no other devices connected to the EVM:
In EnergyTrace (3.6V source from MSP-FET) I get a very high minimum sleep mode current of ~0.3 mA which is way over the stated sleep mode current(1uA) in mentioned guide above. Using the battery and multimeter I get the value between ~0.1 and 0.2 mA, guessing that the MSP-FET also draws some current in the DC-DC converter...?
What should I debug?
Thanks in advance!
Best regards,
Thibault