This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-THREEPHASEMETER-F6779: Msp430f6779

Part Number: TIDM-THREEPHASEMETER-F6779
Other Parts Discussed in Thread: MSP430F6779

Hello,

            I am using MSP430f6779 for energy meter.i need to implement Half duplex UART communication on9600 baud rate . Now am i want to increase the baud rate from 9600 to 115200.So please suggest  the configuration.Which Crystal i have to use.Is 32 Khz crystal is able to generate 115200 buad rate?

Thanking you,

Nilesh Motawala

  • Hello Nilesh,

    For information on how to generate UART baud rates, as well as suggested settings for different input lcocks and baud rates, please see Chapter 39, eUSCI in UART mode in the device User Guide. Particularly sections 39.3.9 and 39.3.13.

**Attention** This is a public forum