Hello all,
I am trying to get comfortable with the Captivate Keypad , Captivate PGMR and the Captivate design center (CDC). While the documentation is great I am running into troubles with the advertised I2C communication capabilities of the captivate programmer. If I am opening the captivate keypad example, leave everything unchanged and use UART as default communication, generate the source out of captivate design center and upload it to the keypad everything is working as expected. If I am just changing the communication channel from UART to BULK_I2C, create the source and upload it again I can connect to the HID but am not getting any data within the captivate design center nor on the device. Am I am missing something here?
According to the documentation the HID (programmer) should automatically switch to I2C when selected as preferred communication in the CDC. I have the same behavior also on a custom sensor board with the same MCU as on the Keypad as well as on a Windows and Mac computer.
I hope someone can give me a hint or explain to me why the generated source with selected I2C is not working ootb as stated in the documentation. Thank you for your help!