dear champion
I want to know the highest speed,in the first page of datasheet,you said 10MHz.
but it can be clocked by SMCLK, if i set SMCLK 16MHz, what will my SPI.
Best Regards
Emma
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
dear champion
I want to know the highest speed,in the first page of datasheet,you said 10MHz.
but it can be clocked by SMCLK, if i set SMCLK 16MHz, what will my SPI.
Best Regards
Emma
From section "31.3.6 Serial Clock Control" of the User's Manual:
"With UCBRx = 0, the maximum bit clock that can be generated in master mode is BRCLK."
From Figure 31-1 on page 796 of the User's Manual, BRCLK is the output of the mux that includes SMCLK.
So, yes, you can run your SPI at 16MHz. However, your connection and peripheral device might not support this speed.
Hi Emma,
For the first page message 10MHz, I still need to check with our system owner to give you confirmation.
Let me clarify the concept for highest rate:
The clock source which input to SPI is the feUSCI = 16MHz for maximum, which is the clock rate of SPI module runs. The bit rate is the fUCXCLK which is the rate of the SPI bus clock.
But the SPI highest bit rates is depends on both master and slave side, which means both side devices of the SPI bus. You could calculate the fUCxCLK by the equation in Table 5-19's note1.
**Attention** This is a public forum