This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

BOOSTXL-BATPAKMKII: charge while using

Prodigy 10 points

Replies: 1

Views: 73

Part Number: BOOSTXL-BATPAKMKII

can the battery be charged and use at the same time?

  • Hi,
    please let me rephrase your question a bit.
    Yes, the connected application/launchpad can continue its operation also during charging of the battery. But of course when the battery is charged, the necessary current for the application is not coming out of the battery, as it wouldn't be charged, but it is delivered from the connected USB device, which is supplying the Launchpad and the necessary current for charging the battery.

    Best regards
    Peter

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.