I get message "configuration update failed"
When I try to do ‘Request Update’. The update failed message show-up as below picture.
How can I fix it?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I get message "configuration update failed"
When I try to do ‘Request Update’. The update failed message show-up as below picture.
How can I fix it?
Lee,
Are you rebuilding the code in CCS before loading to the board? Can you take a picture of what your board jumper configuration looks like? I would suggest removing JP3 and J31 if you are using this for water.
Hi Eddie:
I didn't rebuild the code in CCS . My board jumper configuration is shown in the following figure:
In order to use the EVM430-FR6043 for water flow .The hardware changes:
1.replace R75 and R80 with 1000pF cap, replace R77 and R78 with 200 ohm resistor, and place 0 ohm resistors on R76 and R79.
2.remove JP3 and J31
If I want to use EVM430-FR6043 for water flow , what changes need to be made in software or hardware?
Thanks and look forward to your reply!
You could also remove JP4 and JP5, although this is not the cause of your issue. It sounds like a software issue. I recommend you build the water code and use that. As an alternative, I have built the code and attached the binary if you want to try and load this one. MSP430FR6043EVM_USS_Water_Demo.txt
**Attention** This is a public forum