Other Parts Discussed in Thread: MSP430F5659, MSP430F5658, MSP430F6658
Hi,
I still struggling with getting the USB BSL to work. I changed the constant from 0F 05 0F 03 11 02 17 01 to 0F 05 0F 03 11 04 17 01 in the firmware for the BSL code as described in a previous post. According to the users manual 02 11 is the BSL code setting for 4MHZ and 16MHZ should require values of 04 11, if I read the users manual correct.
However it doesn't work. When I try to run the BSL as is, I get a message from my PC that there is an unknown connection. I expect this because neither of the 4,8,12 or 24Mhz tries works and the device cannot enumerate. However when I change the 02 to an 04, I still get the same message saying an unknown device is connected as soon as I jumpt to location 1000.
Any ideas of what I'm doing wrong??
Thanks,
Jerry