Tool/software: TI C/C++ Compiler
Using the UniFlash Packager to create a BAT file that I can run to program my device. The question I have is the dslite.bat file opens a command window and programs and verifies the programming then closes the command window. Is there something I can place in the dslite.bat that will keep the command window open so that I can scroll through and review the programming/verify process. Tried cmd \k, pause, @pause at the end of the dslite.bat file but that doesn't work, I may not be placing these in the right place in the .bat file. Need some suggestions on how to keep the command window open so I can review the process. Need to add something to the dslite.bat file since this will be given to service people for updating firmware, and if there are issues I need them to tell me what is in the command window.