Part Number: MSP432P401R
Tool/software: Code Composer Studio
Hi All,
I recently upgraded to CCS9 and after getting my projects setup and compiling, I tried to upgrade CCS9, because there were some updates, including a JLink one. I have a JLink programmer, but don't usually use it. The upgrade had some problems, but I went on to try to flash an EXP-MSP432P401R red board. I got the following error:
Sketch uses 40216 bytes (15%) of program storage space. Maximum is 262144 bytes.
Global variables use 25740 bytes (39%) of dynamic memory, leaving 39796 bytes for local variables. Maximum is 65536 bytes.
DSLite version 8.2.0.1400
Configuring Debugger (may take a few minutes on first launch)...
Initializing Register Database...
Initializing: CS_DAP_0
Executing Startup Scripts: CS_DAP_0
Initializing: CORTEX_M4_0
Executing Startup Scripts: CORTEX_M4_0
Connecting...
fatal: CS_DAP_0: Error connecting to the target: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the ReadMe.txt file there for instructions. (Emulation package 8.0.27.9)
Failed: Operation was aborted
the selected serial port Failed: Operation was aborted
does not exist or your board is not connected
Sketch uses 40216 bytes (15%) of program storage space. Maximum is 262144 bytes. Global variables use 25740 bytes (39%) of dynamic memory, leaving 39796 bytes for local variables. Maximum is 65536 bytes. DSLite version 8.2.0.1400 Configuring Debugger (may take a few minutes on first launch)... Initializing Register Database... Initializing: CS_DAP_0 Executing Startup Scripts: CS_DAP_0 Initializing: CORTEX_M4_0 Executing Startup Scripts: CORTEX_M4_0 Connecting... fatal: CS_DAP_0: Error connecting to the target: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the ReadMe.txt file there for instructions. (Emulation package 8.0.27.9) Failed: Operation was aborted the selected serial port Failed: Operation was aborted does not exist or your board is not connected
I tried another one, and got the same results.
Finally I tried a brand new board since I had one here, and it has the same error. I moved my CCS9 install folder and reinstalled it. After getting it set up, I still get this error.
Then I tried flashing the board with Energia 21, and got this message from Energia:
Sketch uses 40216 bytes (15%) of program storage space. Maximum is 262144 bytes. Global variables use 25740 bytes (39%) of dynamic memory, leaving 39796 bytes for local variables. Maximum is 65536 bytes. DSLite version 8.2.0.1400 Configuring Debugger (may take a few minutes on first launch)... Initializing Register Database... Initializing: CS_DAP_0 Executing Startup Scripts: CS_DAP_0 Initializing: CORTEX_M4_0 Executing Startup Scripts: CORTEX_M4_0 Connecting... fatal: CS_DAP_0: Error connecting to the target: (Error -260 @ 0x0) An attempt to connect to the XDS110 failed. The cause may be one or more of: no XDS110 is connected, invalid firmware update, invalid XDS110 serial number, or faulty USB cable. The firmware and serial number may be updated using the xdsdfu utility found in the .../ccs_base/common/uscif/xds110 directory of your installation. View the ReadMe.txt file there for instructions. (Emulation package 8.0.27.9) Failed: Operation was aborted the selected serial port Failed: Operation was aborted does not exist or your board is not connected
Does anyone have any ideas?
Thanks,
Rob