This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/MSP432P401R: MSP432P401R

Part Number: MSP432P401R

Tool/software: Code Composer Studio

Hello sir, i have to select microcontroller for portable battery power medical deivece.for that  i m looking for  a microcontroller with 16 bit SAR ADC with 1 MSPS and built in BLE Hardware. SO, please suggest me.

is there any MSP microcontroller comes with built in BLE Hardware?

  • There is no direct match for what you are attempting to do. The MSP432 is a 14-bit SAR ADC which provides 13.2 bit ENOB and is better than some 16-bit converters. There is no MSP with a radio integrated, an exception would be the CC430 but this is SUB-1Ghz.

    Please look into this TI Design based upon the CC2640 and ADS8885. www.ti.com/.../tida-01012
    The ADS8885 could be replaced with the ADS8860.

    Regards,
    Chris

**Attention** This is a public forum