Other Parts Discussed in Thread: MSP430FR2433
Hello All!
I am building a simple SSD1306 OLED library on MSP-EXP430FR2433 Launchpad. I am using SPI as serial communication interface.
I made it run and development was going well until I faced a weird issue with P2.7
I was using P1.5 for RESET signal of SPI SSD1306 OLED controller. Then I needed to use that pin for UART RX functionality on eUSCIA0. So I changed the reset signal to P2.7 pin. Right after this, I cannot get image on my OLED display. The reset signal is ONLY used in initialization section routine of my library. And the weird thing, if I change the RESET line back to P1.5, bingo it works again.
I checked the datasheet to see some difference btw P1.5 and P2.7, could not find any. Also I connected P2.7 to onboard led with a jumper wire, port seems functioning because led responds as I expect.
I use CCS cloud ide, so compiler version and driverlib version is the default ones on cloud.
Thanks in advance!