This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-EXP430FR5739: Application UART serial com doesn't work in Windows 10 EDUCATION

Part Number: MSP-EXP430FR5739
Other Parts Discussed in Thread: CC3220SF-LAUNCHXL

Hi there,


I've programmed an MSP-EXP430FR5739 launchpad with a simple application to send data by the serial UART. I connected the launchpad to a pc using the USB cable and I used the terminal included in CCS 9 to read this data using a serial virtual com.

When I plug the launchpad in a PC with Windows 10 HOME, it works. I can read the data sent by the microcontroller.

When I plug the launchpad in a PC with Windows 10 EDUCATION, it doesn't work, that is, nothing is received.

I tried with several PCs, launchpads and cables, and also with putty and Hercules terminal, and the behaviour is always the same: Windows 10 HOME works, Windows 10 EDUCATION doesn't work

Even I've checked with two PCs with Windows 10 EDUCATION, connecting them using two USB-Serial adapter and I can send and receive data to/from each PC using the terminal included in CCS 9.

Is there a problem with the MSP430 Application UART driver in Windows 10 EDUCATION?

Thanks for your help,

Toni.

**Attention** This is a public forum