This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/EVM430-FR6047: CCS/EVM430-FR6047: ADC capture waveform

Part Number: EVM430-FR6047

Tool/software: Code Composer Studio

Hello, TI's USS technical expert, I encountered the following problems during the use of EVM430-FR6047:

1. Capture the ADC and the waveform is qualified under the condition that the water inside the pipe is full and not flowing, as shown in the following figure:

2. When the water in the pipe is flowing at 50LPM, the ADC capture waveform is not qualified, as shown in the following figure:

3, Supplementary Description: When the water in the pipe flow to 5LPM, the ADC capture waveform is also qualified, I do not know where the problem?

**Attention** This is a public forum