Hi
I am working on Ethernet-based IO Control Example of MSP432E401Y SDK.
The example uses a UART peripheral for printing the details on a console.
But the way they have initialized the UART peripheral and used it is different from usual.
I am a beginner and unfamiliar with such technique.
I wish to use a UART peripheral say UART4 in the example but as I include the code required along with the libraries the below errors show up.
How can I correct this or How can initialize a UART peripheral of my choice in the Ethernet Based IO Control example itself.
Below is the screenshot of the error message shown.