hi,
We want to use the MSP432E4's BSL to do the FW upgrade via Ethernet. We got some questions need your help:
1.In SLAU746A "MSP432E4 SimpleLink™ Microcontrollers Bootloader(BSL)", I saw the source code of MSP432E4's BSL is provided, but where to get the source code?
2.will the MSP432E4 get auto reset after the Ethernet BSL FW upgrade?
3.I saw it's based on DHCP, if my system is fixed IP, does it also support? Or where should be modified to support the fixed IP?
4. Does the function of Ethernet BSL stored in ROM? If it does, can i still possible to modify something in it?
Thank you.