Other Parts Discussed in Thread: EVM430-F6779, ISO7421, MSP-ISO, MSP-FET
Hi team,
I am working on a demo with the EMDC and EVM430-F6779.
I follow the guidelines and were able to get the HID bridge which is the F5529LP connected to the GUI. However, the EVM didn't. I can only see the text "HID Connected" at the bottom left of the GUI. Compares to the guidelines, the only difference I made is the isolation board. I am waiting for the MSP-ISO board shipped. In the meantime, I created a simple circuit using ISO7421 as shown in the picture below.
On the SW side, I programmed the F6779 EVM with the image. I even tried to generate code from the example project (EVM430-F6779_CT_3V_3C_50Hz), import it to CCS, build and download to the board.
By using an oscilloscope I was able to see short pulses at RX_EN pin on the EVM, but there was nothing on the TX_EN.
What else should I check?