Part Number: MSP-FET430UIF
Tool/software: Code Composer Studio
I'm working with "Code Composer Studio v9" and "MPS430 USB-Debug-Interface MSP-FETU430IF" in Win7.
When I made the CCS project, I defined a "TI MSP430 USB1 [Default]" connection with MSP430F1611 microcontroller.
The project contains several .c and .h files, however with debug launching it seems to work properly.
There aren't error or warning messages. The program goes in running (Resume) automatically and the green led (power) is on, while the red led (mode) blinks. In console appears the Flash/FRAM and RAM usage.
Approximately, after a minute the green and red leds are on but the hardware doesn't work. It seems like if the program has not been loaded/uploaded.
What could be?
Best regards,
Matteo