Other Parts Discussed in Thread: MSP-EXP430G2ET,
I am working on an embedded design that will use the MSP430 as the main controller. Specifically, I plan on using this part. I am currently using the PDIP version of the MSP430G2553. I have this MSP430 on a perfboard and I can program it via SPI-By-Wire when I use the MSP-EXP430G2ET LaunchPad emulator as the programmer.
If I have the same external bypass caps and Reset resistor (as per the datasheet) and a header for the Power, GND, Reset, and Vtest pins, can I also program the MSP430 I linked above via SPI-By-Wire? I am pretty sure I can because it works with the PDIP package, I just want to double check before I commit myself to a PCB.
Follow up question, is it possible to use the MSP-EXP430G2ET LaunchPad emulator to program other MSP430s via SPI-By-Wire so long as I select the proper target board in the IDE? Right now I am only using the G2553 because it is what came with the LaunchPad. Another MSP430 device might actually be better for my design...