Part Number: MSP-EXP430F5529
Tool/software: Code Composer Studio
Hello ,
I have a quick question. Is their a way to receive a multiple bytes without knowing how many they are through UART .and retransmit all of these bytes
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP-EXP430F5529
Tool/software: Code Composer Studio
Hello ,
I have a quick question. Is their a way to receive a multiple bytes without knowing how many they are through UART .and retransmit all of these bytes
i wrote the following code in the main function but i didn't receive the whole characters
what i missed please?
while(1){
unsigned char x;
char *receive;
unsigned int i;
while (!(UCA0IFG&UCRXIFG)); // USCI_A0 RX buffer ready?
{
receive = (char*)malloc(x* sizeof(char) ); /* allocating memory dynamically */
for (i=0; i<x;i++){
receive[i]=UCA0RXBUF;
// free(receive);
}}
while(!(UCA0IFG&UCTXIFG));{
for (i=0; i<x;i++){
UCA0TXBUF=receive[i];}
}
free(receive);
}
Hi Ali,
You can receive every single byte and transmit that byte immediately.
/* --COPYRIGHT--,BSD_EX * Copyright (c) 2012, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ******************************************************************************* * * MSP430 CODE EXAMPLE DISCLAIMER * * MSP430 code examples are self-contained low-level programs that typically * demonstrate a single peripheral function or device feature in a highly * concise manner. For this the code may rely on the device's power-on default * register values and settings such as the clock configuration and care must * be taken when combining code from several examples to avoid potential side * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware * for an API functional library-approach to peripheral configuration. * * --/COPYRIGHT--*/ //****************************************************************************** // MSP430F552x Demo - USCI_A0, 115200 UART Echo ISR, DCO SMCLK // // Description: Echo a received character, RX ISR used. Normal mode is LPM0. // USCI_A0 RX interrupt triggers TX Echo. // Baud rate divider with 1048576hz = 1048576/115200 = ~9.1 (009h|01h) // ACLK = REFO = ~32768Hz, MCLK = SMCLK = default DCO = 32 x ACLK = 1048576Hz // See User Guide for baud rate divider table // // MSP430F552x // ----------------- // /|\| | // | | | // --|RST | // | | // | P3.3/UCA0TXD|------------> // | | 115200 - 8N1 // | P3.4/UCA0RXD|<------------ // // Bhargavi Nisarga // Texas Instruments Inc. // April 2009 // Built with CCSv4 and IAR Embedded Workbench Version: 4.21 //****************************************************************************** #include <msp430.h> int main(void) { WDTCTL = WDTPW + WDTHOLD; // Stop WDT P3SEL |= BIT3+BIT4; // P3.3,4 = USCI_A0 TXD/RXD UCA0CTL1 |= UCSWRST; // **Put state machine in reset** UCA0CTL1 |= UCSSEL_2; // SMCLK UCA0BR0 = 9; // 1MHz 115200 (see User's Guide) UCA0BR1 = 0; // 1MHz 115200 UCA0MCTL |= UCBRS_1 + UCBRF_0; // Modulation UCBRSx=1, UCBRFx=0 UCA0CTL1 &= ~UCSWRST; // **Initialize USCI state machine** UCA0IE |= UCRXIE; // Enable USCI_A0 RX interrupt __bis_SR_register(LPM0_bits + GIE); // Enter LPM0, interrupts enabled __no_operation(); // For debugger } // Echo back RXed character, confirm TX buffer is ready first #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector=USCI_A0_VECTOR __interrupt void USCI_A0_ISR(void) #elif defined(__GNUC__) void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void) #else #error Compiler not supported! #endif { switch(__even_in_range(UCA0IV,4)) { case 0:break; // Vector 0 - no interrupt case 2: // Vector 2 - RXIFG while (!(UCA0IFG&UCTXIFG)); // USCI_A0 TX buffer ready? UCA0TXBUF = UCA0RXBUF; // TX -> RXed character break; case 4:break; // Vector 4 - TXIFG default: break; } }
Ling
Hi Gary,
i wrote the following code in the main loop and i checked the received data i received all of them correctly
while(1){
char *receive;
unsigned int i;
receive = (char*)malloc(120); /* allocating memory dynamically */
while (!(UCA0IFG&UCRXIFG)); // USCI_A0 RX buffer ready?
{
for (i=0; i<120;i++){
while (!(UCA0IFG&UCRXIFG)); // USCI_A0 RX buffer ready?
receive[i]=UCA0RXBUF;
}
but when i tried to re-transmit what i received, the code transmit the data more than one time and sometimes with a missing bytes
the transmit code as following
#if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__)
#pragma vector=USCI_A0_VECTOR
__interrupt void USCI_A0_ISR(void)
#elif defined(__GNUC__)
void __attribute__ ((interrupt(USCI_A0_VECTOR))) USCI_A0_ISR (void)
#else
#error Compiler not supported!
#endif
{
char *receive1;
unsigned int n;
receive1 = (char*)malloc(120); /* allocating memory dynamically */
while (!(UCA0IFG&UCTXIFG)); // USCI_A0 TX buffer ready?
{
for (n=0; n<120;n++){
while (!(UCA0IFG&UCTXIFG)); // USCI_A0 TX buffer ready?
UCA0TXBUF=receive1[n];
}
}
}
**Attention** This is a public forum