Part Number: MSP430F2618-EP
Dears:
After welding and baking at 120 C for 2 hours, can MSP430F2618-EP bear it?
Will Flash flip and cause program errors or other problems?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Luck,
This violates the absolute maximum ratings.
Storage temperature: Unprogrammed device --55C to 150C
Programmed device --40C to 105C
There is possibility that it could corrupt the flash. It would be recommended to program the device after this step.
If this answers your question, please click "This Resolved My Issue"
Regards,
Wade
As already noted, this violates the absolute max ratings, and it can affect device.
There is possibility that it could corrupt the flash. It would be recommended to program the device after this step.
If this answers your question, please click "This Resolved My Issue"
Regards,
Wade
Hi Wade:
I am so sorry for making your misunderstanding.
Customer knows don't program the device since the temperature of Programmed device is lower and can not bear the operation.
If they do not program the device. After welding and baking at 120 C for 2 hours, can MSP430F2618-EP bear it.
Is the Time so long to damage these device?
Pls. kindly help to give some advice.
120C for 2 hours will not damage an unprogrammed device.
Programming device after this condition is required to insure proper programming.
This is the meaning of the absolute maximum ratings for programmed and un-programmed devices.
Hopefully this clears this up.
Regards,
Wade
**Attention** This is a public forum