Other Parts Discussed in Thread: LMX2595,
Tool/software: Code Composer Studio
Respected sir,
1) I am working on MSP430F5229 to set the programmable divider value which is in feedback path of VCO and phase frequency detector of LMX2595 ic by using its delta sigma modulator. Can I get the sample format of the code of MSP430F5229 such that i can take it as reference and build as per my designed synthesizer. I need to set the divider ratio value to 42.5 and load several registers with the values obtained from TICS pro software to function as per the design. Now to load these values in the MSP430F5229 can I get the sample code for reference.
2) As MSP430F5229 is a 16 bit controller and the data which i get from the TICS pro software is 32 bit long. As I found that LMX29595 is compatible with the M430F5229 but it has 16 bit registers nowhow could I overcome this problem, how to use two 16 bit controllers to make use it as 32-bit.
thanks in advance