Part Number: MSP-FET430UIF
Hi,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: MSP-FET430UIF
Hi,
Hello,
The interface communication error could be the result of a variety of issues. It could be from connections being routed incorrectly in the schematic, the programmer itself, the passives around the MCU (specifically the reset line) might not be wired correctly, etc....
Could you provide schematics for the 2 boards you are using so that we can see if the signals are being routed correctly?
Best regards,
Matt
Hi,
The issue was solved by updating the libmsp430.so as per the instructions from the link https://dlbeer.co.nz/articles/slac460y/index.html after doing this the "tilib" worked well for some days then again it shows the same error(interface communication error).
But the whole arrangement worked well in CCS(windows).At the same time CCS 7.0.0 in ubuntu shows the "interface communication error".
Hari,
The fact that it can be working for an extended period of time with no issues and then all of a sudden stop working would initially point me in the direction of some sort of hardware related issue causing sporadic device initialization errors. Are you able to confirm this same phenomena with alternate boards, a different programmer, or perhaps another computer? I am trying to figure out where we can isolate the problem to.
Best regards,
Matt
**Attention** This is a public forum