Using SimpleLink version 3.20.
In the httpget_MSP_EXP432E401Y_tirtos_ccs_syscfg, I setup a static IP using syscfg. Then followed the steps in the original question, and even trying to set the breakpoint and to delay 2 seconds after SiNetIf_add call, I keep getting the following error code:
"Error! code = -2006, desc = httpTask: connect failed"
I know the static IP I programmed works because I can run the tcpecho example by programming the static IP the same way.
The function "CfgAddEntry(0, CFGTAG_SYSINFO, CFGITEM_DHCP_DOMAINNAMESERVER, 0, sizeof(uint32_t), (unsigned char *)&ip, 0);" always returns 0. Looking at config.c the documentation header states the following: