Hello,
I'd like to ask if the following connection of Vcore(MSP430F5437A pin#49) is correct. Please refer to the picture.
VCORE doesn't look like being connected correctly. The datasheet says as follows:
CVCORE : Recommended capacitor at VCORE 470nF.
All voltages referenced to VSS. VCORE is for internal device use only. No external DC loading or voltage should be applied.
Can you please check and give us an advice?
Thanks, HJ.