This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR6043: GUI UPS/DNS Gap timing

Part Number: MSP430FR6043

Hello,
I had a look on to the "UPS and DNS Gap" and "UPS0 to UPS1 Gap" timings with a scope. The timing are a higher than configured with the GUI.
I set the UPS/DNS gap to 8000us but measure 9.7ms. The UPS0/UPS1 gap is set to 150ms but measured 187ms.

GUI version: 02_20_00_19
SW version: 02_20_00_12

Regards, Holger

**Attention** This is a public forum