Other Parts Discussed in Thread: MSP430FR6047,
Hi,
We are a startup based in Netherlands. We want to design and develop ultrasonic water meters based on the MSP430FR6047 MCU for the Indian and east european market segment. But we are from embedded firmware background and do not have domain knowledge on water measurement.
So, we want help from you in choosing the right transducers to be used with MSP430FR6047 MCU to measure the speed and amount of water flow.
Also we do not want to cut the pipes. Is it possible to make residential ultrasonic water meters (diameter of pipes are 15mm or 20mm) which can be clamped on top of the pipes without cutting them so that water supply is not interrupted while installation.
We also want advise on where to buy the cheap and reliable transducers which can be connected to the EVM430-FR6047 evaluation board (based on MSP430FR6047 MCU) so that we can start prototyping the ultrasonic water meters and make them and test them quickly.
Looking forward to your help and guidance.
Thanks and Regards,
Sritam Paltasingh.