Dear Champs,
Does MSP430FG437 have internal temp sensor calibration data or TLV table for ADC calibration data?
If you have any concern, please feel free to let me know.
Thanks a lot.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Champs,
Does MSP430FG437 have internal temp sensor calibration data or TLV table for ADC calibration data?
If you have any concern, please feel free to let me know.
Thanks a lot.
Hi Janet,
Thanks for posting your question to E2E. The MSP430FG437 does have an integrated temperature sensor as part of the ADC12 module. Here's a figure copied from the user's guide illustrating how channel 1010b is connected to the temperature sensor. Section 28.2.8 in the user's guide discusses how to use it.
Unlike some of our newer devices, I couldn't find TLV data available in the MSP430FG437 datasheet. I did find a code example that demonstrates how to use the internal temperature sensor, but it does not show how to calibrate the sensor. Thus, I suspect that you'll need to calibrate (eliminate the offset of) the temp sensor manually for each device.
/* --COPYRIGHT--,BSD_EX * Copyright (c) 2012, Texas Instruments Incorporated * All rights reserved. * * Redistribution and use in source and binary forms, with or without * modification, are permitted provided that the following conditions * are met: * * * Redistributions of source code must retain the above copyright * notice, this list of conditions and the following disclaimer. * * * Redistributions in binary form must reproduce the above copyright * notice, this list of conditions and the following disclaimer in the * documentation and/or other materials provided with the distribution. * * * Neither the name of Texas Instruments Incorporated nor the names of * its contributors may be used to endorse or promote products derived * from this software without specific prior written permission. * * THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" * AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, * THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR * PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR * CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, * EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, * PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; * OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, * WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR * OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, * EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. * ******************************************************************************* * * MSP430 CODE EXAMPLE DISCLAIMER * * MSP430 code examples are self-contained low-level programs that typically * demonstrate a single peripheral function or device feature in a highly * concise manner. For this the code may rely on the device's power-on default * register values and settings such as the clock configuration and care must * be taken when combining code from several examples to avoid potential side * effects. Also see www.ti.com/grace for a GUI- and www.ti.com/msp430ware * for an API functional library-approach to peripheral configuration. * * --/COPYRIGHT--*/ //****************************************************************************** // MSP-FET430P430 Demo - ADC12, Using the Temperature Sensor // // This example shows how to use the intergrated temperature sensor to measure // temperature. When the temperature diode channel (A10) is selected for // conversion, the internal reference is automatically turned on as the source // for the sensor. Note however, that it is NOT automatically selected for the // conversion. Any available reference can be used for the conversion. In // this example, a single conversion is performed of the temperature diode. // The temperature is then calculated in degrees C and F, based on the A/D // conversion value. Test by setting and running to a break point at "_NOP()". // To view the temperature open a watch window with the debugger and view DegC // and DegF. // ACLK = n/a, MCLK = SMCLK = default DCO, ADC12CLK = ADC12OSC // // Note: This example does not perform a calibration on the temperature sensor // A calibration of the temperature senosr may be necessary in an application. // see the device datasheet for the temperature sensor specification. // // MSP430FG439 // --------------- // | | // |A10 (Temp) | // | | // // M. Mitchell // Texas Instruments Inc. // Feb 2005 // Built with CCE Version: 3.2.0 and IAR Embedded Workbench Version: 3.21A //****************************************************************************** #include <msp430.h> static unsigned int ADCresult; static volatile unsigned long int DegC, DegF; int main(void) { volatile unsigned int i; WDTCTL = WDTPW+WDTHOLD; // Stop watchdog timer ADC12CTL0 = ADC12ON+REFON+REF2_5V+SHT0_6; // Setup ADC12, ref., sampling time ADC12CTL1 = SHP; // Use sampling timer ADC12MCTL0 = INCH_10+SREF_1; // Select channel A10, Vref+ ADC12IE = 0x01; // Enable ADC12IFG.0 for (i=0; i<0x3600; i++) // Delay for reference start-up { } ADC12CTL0 |= ENC; // Enable conversions __enable_interrupt(); // Enable interrupts while(1) { ADC12CTL0 |= ADC12SC; // Start conversion __bis_SR_register(LPM0_bits); // Enter LPM0 // DegC = (Vsensor - 986mV)/3.55mV // Vsensor = (Vref)(ADCresult)/4095) // DegC -> ((ADCresult - 1615)*704)/4095 DegC = ((((long)ADCresult-1615)*704)/4095); DegF = ((DegC * 9/5)+32); // Calculate DegF __no_operation(); // SET BREAKPOINT HERE } } #if defined(__TI_COMPILER_VERSION__) || defined(__IAR_SYSTEMS_ICC__) #pragma vector=ADC12_VECTOR __interrupt void ADC12ISR (void) #elif defined(__GNUC__) void __attribute__ ((interrupt(ADC12_VECTOR))) ADC12ISR (void) #else #error Compiler not supported! #endif { ADCresult = ADC12MEM0; // Move results, IFG is cleared __bic_SR_register_on_exit(LPM0_bits); // Clear LPM0 }
Regards,
James
**Attention** This is a public forum