This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP-GANG: unlock the MSP432 MCU by MSP-GANG

Part Number: MSP-GANG

I have  a MSP-GANG Programmer  and I want use this device to unlock a MSP432 MCU which was locked by set JTAG_SWD_LOCK_SECEN.

I know use MSP-GANG window software can unlock it by click "Clear Locked Device" button .

But in this way , I need install the windows software. 

I want just use the MSP-GANG device like the Standalone mode to unlock the MCU.

Is it possible that I make an image just do unlock the MCU process and download it into MSP-GANG?

Or any other ways to unlock the MCU just use the MSP-GANG device . 

Thanks!

  • user1600444,

    All protection options are described in the MSP432 Technical Reference Manual and are implemented by programming the flash mailbox. The MSP-GANG can program the flash mailbox according to user settings or directly from code file.

    See Section 4.8 in the MSP432 TRM here.

    BR,

    Seong

**Attention** This is a public forum