Other Parts Discussed in Thread: TIDM-THREEPHASEMETER-F6779, MSP430F6779A
Part Number for Crystal used in EVM430-F6779. Its component XT1.
Also if possible to have BOM for EVM430-F6779.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number for Crystal used in EVM430-F6779. Its component XT1.
Also if possible to have BOM for EVM430-F6779.
Hello,
The BOM for EVM430-F6779 can be found on the TIDM-THREEPHASEMETER-F6779 product page (essentially a reference design that uses the EVM430-F6779). On that page, the BOM can be found under the "Design files" section towards the bottom. Then, search for "XT1" inside that document. The part number is there.
Regards,
James
By the way, are you still using the Energy Measurement Design Center (EMDC) in your design? Also, make sure to use the A-version device, MSP430F6779A, in your final design.
Regards,
James
Yes we are using Energy Measurement Design Center (EMDC) in our design. Kept to the principle of using the metering code produced by EMDC.
I noticed that the crystal in BOM dco is 32.7680KHZ but i believe one used on EVM is 25. KHZ.
Bilal.m.Ahmad said:Yes we are using Energy Measurement Design Center (EMDC) in our design. Kept to the principle of using the metering code produced by EMDC.
That's great to hear. Thanks for letting us know.
Bilal.m.Ahmad said:I noticed that the crystal in BOM dco is 32.7680KHZ but i believe one used on EVM is 25. KHZ.
Interesting. It should also be 32.768 kHz. You could check by outputting the frequency through I think it's the ACLK pin. If you measure the crystal directly using probes, the extra capacitance can skew the measurements. Routing the clock signal through the MCU allows you to measure it without affecting the capacitance. Hope that helps!
Regards,
James
Hi Bilal,
Sorry for misunderstanding. Yes, you're correct that the EMDC GUI configures the MSP430F6779A's internal DCO for 25.165MHz operation. The DCO supplies the system clock (SCLK) and master clock (MCLK). The external crystal, XT1, is normally 32.768 kHz and used for ACLK. This low-frequency crystal can be used for low-power modes, clocking the RTC and also as the FLL reference clock for the internal DCO. I hope that makes more sense.
Regards,
James
**Attention** This is a public forum