SDK setup:
1. simplelink_sdk_ble_plugin_3_20_00_24 for MSP432E401Y
2. simplelink_cc2640r2_sdk_3_20_00_21
I am planning to use MSP432E401Y as the Application processor and CC2640R2 as the Network processor.
I want to use SPI as the serial link between both the processors.
Question:
1. By including "NPI_USE_SPI" symbol in the "simple application processor" example will I be able to use the MSP432 with SPI as the serial link?
2. What are the changes required in the "simple application processor" example to use it with SPI serial link?
3. As "npi_tl_spi.c" is not part of the "/source/ti/npi" folder. Do we have to implement the "npi_tl_spi.c"? After writing this Do we need to rebuild the SDK? If SDK rebuild is required what is the method to rebuild the SDK?
I will be using the "cc2460r2lp_simple_np_spi_pm_sbl.hex" for the CC2640R2 processor when using SPI as the serial link.
4. What are the changes required in the "simple_np_cc2640r2lp_app" project to use it as SPI based serial link?
I didn't find documentaion related to the porting of both the projects to SPI based serial link. It would be helpful if I get any resource which describes the procedure to use SPI as the serial link in a ble_plugin project.
Thank You.