Part Number: MSP430F5529
Tool/software: Code Composer Studio
Hi all,
While I was fiddling around with the GPIO input ports, I tried to use the P1.1 pushbutton of the MSP430F5529LP LaunchPad with the pull-up configuration, all worked fine and good, with all the necessary adjustments. On the other hand, when I try to use the pull-down resistor configuration, the P1IN register does not change to 1 when I press the pushbutton. I followed the instructions on the User Guide (SLAU208) - setting the respective bit in P1OUT to 0 in order to use the pull-DOWN configuration on the pin, and enabling the respective P1REN bit to 1 in order to enable such resistor. Below are the codes for the pull-up and for the pull-down configurations, where the latter does not work. I am very confused.
#include <msp430.h>
#define LED BIT0
#define BTN BIT1
/**
* main.c
*/
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer
P1DIR |= LED;
P1DIR &= ~BTN;
P1OUT |= BTN | LED; // set as pull-up and LED initially on
P1REN = BTN; // enable pull-up resistor
while(1) {
if((P1IN & BTN) != 0)
P1OUT ^= LED;
}
return 0;
}
#include <msp430.h>
#define LED BIT0
#define BTN BIT1
/**
* main.c
*/
int main(void)
{
WDTCTL = WDTPW | WDTHOLD; // stop watchdog timer
P1DIR |= LED;
P1DIR &= ~BTN;
P1OUT &= BTN | LED; // set as pull-down and LED initially off
P1REN = BTN; // enable pull-down resistor
while(1) {
if((P1IN & BTN) != 0)
P1OUT ^= LED;
}
return 0;
}
Thanks in advance.