Hi,
I am using EVM430-FR6047 and using Ultrasonic sensing Design centre application (USS) to interface the same.
I am able to connect the application with the EVM and able to measure the flow .
I checked in the code and found that the communication with the Application is currently through I2C . I want to change it to UART so I modified following line in
comm_config.h file
original line was : #define COMM_SERIAL_INTERFACE (COMM_I2CSLAVE)
changed line is : #define COMM_SERIAL_INTERFACE (COMM_UART)
With this change I have built the code and debugged with the EVM, but now the USS application is not getting connected to EVM . please note that the jumpers RXD , TXD are placed.
How the communication is established on UART?
Thanks in Advance
Suhas