This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP430FR2033: FRAM memory corruption when voltage applied to IO greater than DVCC+0.3V

Expert 3530 points
Part Number: MSP430FR2033

Hi team,

There is a case when I have to hot plug-in/out a MSP430FR2033 board to a system. There are chances that voltage applied to several IOs (eg. UART Tx RxD signals) are greater than the (DVCC+0.3V), eg. when the DVCC is lost first or powered later. According to the Absolute Maximum Ratings table in the datasheet, this can damage the device or corrupt the memory. I verified that.

My question is how I can prevent this from happening?

**Attention** This is a public forum